Hardware, Tools...
Semiconductor & Sensor
Other Comp. & Accessori
 
 LEDs
 
Visitors
Visitors Online : 66
Total accessing: 10307260
 
Filter by Manufacturer

Semiconductor & Sensor >
Images are for reference only, Please See Product Specifications
HC-SR04
Ultrasonic ranging module (Update 25/06/2024)
Part No.:  HC-SR04
Date added::  11/01/2014
Brand:  TAKAMISAWA
Origin:  China
Category:  Ultrasonic sensor
Pricing: 
Quantity (pcs)1 - 9 10 - 24 25+
Unit price (VNĐ) 25,000 24,500 24,000
Product Unit:  pcs
In stock:  53 pcs
Views:  21272
Quantity: 
  1. Product information
  2. Products equivalent

Vendor's Description:

The HC-SR04 ultrasonic sensor uses sonar to determine distance to an object like bats or dolphins do. It offers excellent range accuracy and stable readings in an easy-to-use package. It operation is not affected by sunlight or black material like Sharp rangefinders are (although acoustically soft materials like cloth can be difficult to detect). Similar in performance to the SRF005 but with the low-price of a Sharp infrared sensor.

  • Power Supply :5V DC
  • Quiescent Current : <2mA
  • Effectual Angle: <15°
  • Ranging Distance : 2cm – 500 cm/1" - 16ft
  • Resolution : 0.3 cm
  • Basic use of the HC-SR04 Ultrasonic Sensor

Please see the datasheet for an excellent description of how the sensor operates.

HC-SR04 Datasheet

Using the HC-SR04 with a PICAXE microcontroller

There is a nice tutorial right here at LMR with sample code for using an ultrasonic sensor with a PICAXE 28 project board (thanks Frits!). Do not be disappointed that it’s written for the SRF05 ultrasonic sensor; the sensor operates the same way.

“How to connect SRF05 to Picaxe 28 pin Project board” tutorial

Using the HC-SR04 with an Arduino

There is an Arduino library for the HC-SR04 that offers two ways to use the sensor. To install, download the “Ultrasonic Library” from this page, unzip the release package into your “arduino-0018/libraries/” folder. Open the Arduino IDE and include the library by Sketch-Import library-Ultrasonic . There is also an example sketch in File-Examples-Ultrasonic-UltrasonicDemo.

Ultrasonic Library

The library includes 3 functions:

1. Ultrasonic(int TP, int EP)

This is a initial function for ultrasonic ranging module, choose the pins for module TRIG and ECHO pin. For example:

     Ultrasonic(13,12);

defines the digital pin 13 of Arduino as the TRIG pin of HC-SR04 and pin 12 for the ECHO pin.

2. long Timing()

This function triggers the ultrasonic module and returns the duration that the ECHO pin was held high. For example:

    long time; Ultrasonic hcsr; time = hcsr.Timing();

The distance of the object corelates to the time the ECHO pin is held high. The distance formula is:

     Distance = ((Duration of high level)*(Sonic :340m/s))/2

3. long Ranging(int sys) — (sys : CM / INC)

If you don’t want to change the time into distance yourself, this function will help you get the distance immediately. This function has a parameter (using CM or ICN) that shows the distance in centimeters or inches. This function will call Timing() and you don’t need to use the Timing() before it. For example:

     long distance; Ultrasonic hcsr; distance = hcsr.Ranging(CM);

returns the distance in centimeters.
 

A better, faster, more powerful ultrasonic is availble here:

http://code.google.com/p/arduino-new-ping/
 

jQuery(this).corner();
40KHz Ultrasonic Sensor Pair, 12x16...
Retail Price:
jQuery(this).corner();
HY-SRF05 (30)
Ultrasonic ranging module
Retail Price: